11/7/2020 3:30 PM | |
Posts: 1 Rating: (0) |
HELLO I have in two CU305DP a failure related to the F07900 brake, in a machine with 4 CU305 DP to equal 4 motors. Like a car. But 2 motors had problems with the encoder wires, but now are resolved. When trying to run these two motors are running in the opposite direction and appear the F07900. Do the Starter have any parameter where we define the direction of rotation of the motors???? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/09/2020 09:22:33New subject after splitting |
|
11/9/2020 9:34 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (296) |
Hi, rotating direction can be selected in p1821. |
Best regards, |
|
Follow us on