7/18/2016 9:32 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585) |
Hi, for your first question check the following FAQ for better understanding: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?2. If there is no data connection between two computers with WinCC ES Advanced/Professional or RT Advanced/Professional, the transfer can still be made in WinCC by using a removable medium - check this: With WinCC (TIA Portal) V13, how do you transfer a configuration without a direct data connection to a PC with WinCC Runtime Advanced/Professional?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on