3/4/2014 5:21 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, In the program cycle 83 options are not filled correctly. Please refer the attached file for more information. AttachmentC:\Documents and Settings\ntguest\Desktop\Cycle 83.pdf (534 Downloads) |
3/4/2014 8:13 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please see the attached file.
No it is not possible. Chances of not functioning pre-programed cycles are, either the required data is not filled correctly or by chance cycles are deleted or edited incorrectly. AttachmentC:\Documents and Settings\ntguest\Desktop\CYCLE 84.pdf (213 Downloads) |
3/4/2014 8:58 AM | |
Posts: 9 Rating: (0) |
thankyou, Can you give me an example cycle83 code that i can run to check my controller is reading it correctly?
|
3/5/2014 1:10 AM | |
Posts: 9 Rating: (0) |
below is a copy of the start of the code, as far as i can see it should run cycle83 with no issues. when it stops it throws a 12550 error code. see attached pics for the error wording. is it possible that the machine has forgotten how to run cycles? it works normally if there is no cycles in the code ( 3d milling ) If this sounds like a Machine problem is it easily fixed or how can we go about it? Thanks for your help, Jason _N_SS RAM BASE MILL.NC _MPF ; PATH=/+N_WKS_DIR/_N_FOLDER_WPD ; SIEMENS 810D ;WED. 03/05/201410:26AM ; SIEMENS 810D ; FIRST MACHINE SETUP - Machine Setup - 2 N1 ; T12 DRILL , DIAMETER = 6. , LENGTH =127.) N2 ; T17 DRILL , DIAMETER = 8.5 , LENGTH =127.) N3 ; T11 DRILL , DIAMETER = 13. , LENGTH =127.) N4 ; T1 ENDMILL ROUGH , DIAMETER = 10. , LENGTH =0.) N5 G17 G71 G90 Z500.0 ; FIRST CUT - FIRST TOOL ;JOB 7 HOLE RANDOM POINT PATTERN ;FEATURE DRILL HOLE ; TOOL #12 6. DRILL N6 G00 G54 X64. Y-64. N7 F25.01 S500 M03 N8 T12 M6 N9 Z2.54 M08 N10 F30. N11 MCALL CYCLE83 ( 2.54 ,0. , 2.54 , 15.6 , , 3. , ,1,) N12 X64. Y-64. N13 MCALL ; NEXT CUT - SAME TOOL ;JOB 8 HOLE RANDOM POINT PATTERN ;FEATURE DRILL HOLE N14 S600 N15 G00 G54 X64. Y-20. N16 F30. N17 MCALL CYCLE83 ( 2.54 ,0. , 2.54 , 20. , , 3. , ,1,) N18 X64. Y-20. N19 MCALL [url=http://postimg.org/image/fa5wirr6b/][img]http://s13.postimg.org/fa5wirr6b/photo.jpg[/img][/url] [url=http://postimg.org/image/6hoxv361f/][img]http://s13.postimg.org/6hoxv361f/photo_1.jpg[/img][/url] |
3/5/2014 4:54 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please read & understand the cycle 83 & its variables. Please fill the variables correctly (to understand the variables meaning see theexamples provide in cycle 83) or follow the steps given in remedy action in the attached file, which shall give you the idea about wrong block. AttachmentC:\Documents and Settings\ntguest\Desktop\12550 alarm.pdf (300 Downloads) |
11/18/2016 5:59 AM | |
Posts: 5 Rating: (0) |
I am also facing similar problem of error 12550.Can anyone guide me please. Refer attached files. Can you share what you did to resolve this error. AttachmentError 12550 - SC_TOOL_VALI not defined or option not installed.docx (224 Downloads) |
12/24/2020 3:49 PM | |
Joined: 10/14/2018 Last visit: 6/2/2023 Posts: 2 Rating: (0) |
Your "cycle" or any program "disabled". "Enable" your CALLED program intro "manage" data and load it again. |
Follow us on