Industry Online Support
Technical Forum
4/9/2010 12:33 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User Laujofa wrote: Hello, I try to make the examples from https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=12429336&caller=view (zEn26_02_TF___31xC_Cnt - PWM 1 First steps) I use to simulate the PLCSIM and VAT but the output of the block remanis in 0. The input and hardware configuration is correct. Thank you. |
4/10/2010 2:28 PM | |
Posts: 1 Rating: (0) |
I need some help. I download the example from this page, I folow the step presented on the manual but when I simulate whit VAT and PLCSIM the output don't change. When I change the variable of the input in VAT the input on program is update. The example is zEn26_02_TF_____31xC_Cnt, PWM first time. |
4/12/2010 7:57 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at Which components are not supported by S7-PLCSIM V5.4 Best regards, Hristo Mihalev |
Follow us on