3/7/2022 8:02 AM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating:
|
Hi Wreng, please have a look to this ID Regards |
3/9/2022 10:23 AM | |
Joined: 7/27/2008 Last visit: 11/8/2023 Posts: 25 Rating:
|
Hi Manfred Thank you for your answer. I have tried to make external encoder TO via data block connection as below. Encoder was connected as second encoder of tel 106 at drive axis_2. I have made 'PD_TEL81' for telegram 81, well compiled and then data block for encoder TO. But in the new external encoder TO, the data block is not connected with data block connection. I've wrote 'ExEnc_1.T81.Sensor_1' or 'ExEnc_1.T81.Encoder_1' etc in data block box. What is wrong with me? Here attached some pictures, topology, data block of TO, configure. Thanks Attachmentalsdream.zip (953 Downloads) |
Last edited by: wreng at: 03/09/2022 10:25:12Last edited by: wreng at: 03/09/2022 10:25:34 |
|
3/11/2022 1:36 PM | |
Joined: 12/16/2014 Last visit: 8/27/2025 Posts: 11 Rating:
|
Hi, You have to connect the TO directly to DB_ExEnc.T81. Before that DB_ExEnc must be compiled! The data structure within the variable DB_ExEnc.T81 must be handled corespondingly. The values must be read/written in MC-PreServo / MC-Post-Servo OBs. For this variable you don't need any tag in the tag table. Please refere to following application example - it's very useful! https://support.industry.siemens.com/cs/de/en/view/109741575 |
3/13/2022 3:27 AM | |
Joined: 7/27/2008 Last visit: 11/8/2023 Posts: 25 Rating:
|
Hi bb2126 Thank you for your help It solved well. The problem was the data type PD_TEL81. Thanks again |
Follow us on