11/23/2006 11:00 PM | |
Posts: 5822 Rating: (411)
|
Hello Ashwin, sorry but I am not too deep into S7-200, but maybe the following can help a bit: *** Latest version of the SIMATIC S7-200 Programming Tips 08/03 Check here for Communication. I hope it will help a bit. Best regards J_Bell |
11/24/2006 6:56 PM | |
Posts: 101 Rating: (11) |
Hi, You want to use PPI and s7-200 CPU 224. Ok, first of all you have to divide the 6-byte packet and dump them into the free port address in MicroWin. You may use Interrupts to help constantly read/write the freeport. Also, you need to configure the PPI adapter properly, there are pins on the side that define the bit rate and local/remote transmission that suit your needs. find below the code program that i thought it might be of help for you. the below code is adapted to my own requirements. ***in main*** LDB= SMB86, 16#20
Husam Othman. |
7/15/2009 3:44 PM | |
Posts: 18 Rating: (1) |
can i apply the same thing to cpu 226 REGARD |
Follow us on