1/21/2012 4:00 PM | |
Posts: 344 Rating:
|
There are several parts of the Sinamics System you have to consider: 1. Motor: 1FT7xxxx What kind of feedback do you have on the new motor? Is it DriveCliQ? 2. Motor Module 3. Line Module (and associated line side components). If you are using a Motor Module, it is a DC/AC common bus architecture. 4. Control Unit: CU320-2 is currently used controller 5. Control Unit Flash Card. 5. If the encoder is non-DriveCliQ, an encoder interface module is needed: SMC10, SMC20, SMC30 based on the type of encoder used. 6 Power cables and DriveCliQ cables to connect all components. One sure way to come up with complete parts list is to use Sinamics Sizer program. It will walk you through the system configuration and produce a complete parts list for the system. |
Follow us on