2/23/2023 7:16 AM | |
Joined: 9/1/2022 Last visit: 3/7/2024 Posts: 3 Rating: (0) |
Hello Expert I installed the PCU (50.3b) unit on the machine but the problem is still there the display on the machine is not showing but the machine is fully ready all the motors are working fully the NCU (840dsl) unit of the machine After turning on, the number 6 comes and the run light turns on. The PCU unit doesn't boot seven segments (2E) after it is turned on I think it’s the real problem but I want to know what the (2E) means. I attached some picture please see Regards WK AttachmentPICTURE.docx (342 Downloads) |
Follow us on