3/14/2022 8:59 AM | |
Joined: 1/17/2022 Last visit: 9/4/2023 Posts: 27 Rating: (0) |
Thank you very much for helping me solve a problem How can I add DP-INTERFACE 3RK3511-1BA10 and TOUCH 6AV6647-0AC11-3AXO and CE-58-M 8192/4096 PNO PROFIBUS 10fl/19.5 zb63 to Profibus? I have tried to update the Hardware to no avail I have installed a program SIMATIC WinCC flexible 2008 I could not find the type of serial number for the touch I use a program step 7 v5.5 CPU 412 -2DP ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/14/2022 09:55:46New subject after splitting |
|
3/14/2022 12:02 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello aniial; Te answer to this type of question is not simple. One hint: when you have the part number of a Siemens equipment, put it into the search box at the right of this page, the results page. See the screenshot below for more details. Your first module (3RK3511-1BA10) is a Profibus-DP slave, and the link to the gsd file you need is found in the next link. But note that this is a Safety relay, for full operation you would need a Safety PLC, like a CPU 412F-xxxx. If that works for you, you will find the gsd file for the 3RK3511-1BA10 in this link, on the download for Modular safety Systems: https://support.industry.siemens.com/cs/ww/en/view/113630 Your HMI panel is a KTP600 Basic DP (use the same trick to confirm), itcan be programmed with WinCC Flexible 2008 and can connect to your CPU over Profibus. There are no gsd files for an HMI since it does not act as a slave on the network. It connects as a Master class 2, and all the configurations will have to be done inside WinCC Flexible. https://support.industry.siemens.com/cs/ww/en/view/18797552/1451103371 Your last product is not found in Siemens catalog. A search for a CE-58m-8192/4096 on the web leads to spare parts resellers: https://www.icdcspares.com/product/telestar-ce-58-m-8192-4096-ssi/ Does this description match the product you are working with? There is no mention of communication possibilities for this product. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 03/14/2022 12:04:13 |
|
This contribution was helpful to1 thankful Users |
3/14/2022 1:37 PM | |
Joined: 1/17/2022 Last visit: 9/4/2023 Posts: 27 Rating: (0) |
good greeting Thank you very much for following up on the product part I'm working on
AttachmentCE-58-M PROFIBUS Solid Shaft.pdf (336 Downloads) |
3/14/2022 2:42 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi @NIAL, GSD files can be downloaded on the manufacturers homepage: https://www.tr-electronic.com/service/downloads/file-download hope this helps, regards, |
FCK WAR! |
|
3/17/2022 9:31 PM | |
Joined: 1/17/2022 Last visit: 9/4/2023 Posts: 27 Rating: (0) |
Thank you so much Thank you for helping me and thank you for your interest Greetings and respect to you
|
Follow us on