9/8/2020 9:54 PM | |
Joined: 9/27/2006 Last visit: 10/9/2024 Posts: 12285 Rating: (2685)
|
Hello automata; You continue to ask the same question, over and over, in multiple threads. Please stop and consider the answers that were given, well, the single answer that you were given, over and obver: The AS 410-5H is designed exclusively for PCS 7 (using CFC), it cannot be programmed with Step 7 blocks. Here is how Siemens introduced this new CPU, in 2017: SIMATIC PCS 7 CPU 410-5H Process Automation Released for Delivery https://support.industry.siemens.com/cs/ww/en/view/75407031 “The CPU 410-5H Process Automation is an exclusive product for the SIMATIC PCS 7 process control system and is herewith released for delivery. This CPU enables a very flexible scaling of the modular SIMATIC PCS 7 automation systems AS 410; it can be employed in all domains, i.e. as standard automation system AS 410S, as fault-tolerant automation system AS 410H and as failsafe automation system AS 410 F/FH.” Your choices: - procure a PCS 7 packeage, reprogram all your S7 blocks as PCS 7 CFC instructions blocks.Download this program to the AS 410-5H. - return the AS 410-5H to your vendor if possible, exchange it for a new S7-417-4H, download your existing blocks happily. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/08/2020 22:54:40 |
|
This contribution was helpful to1 thankful Users |
9/9/2020 8:11 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on