12/7/2021 11:11 AM | |
Joined: 4/29/2021 Last visit: 12/28/2021 Posts: 50 Rating: (0) |
Dear Piscean, Yes . Noted .. If am going to purchase advanced CUD unit + profinet module (G00) means I can able to communicate with S71200 (1214 DC) PLC CPU only. Pls clarify this details. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Puli Kutty at: 12/08/2021 07:15:56Last edited by: Jen_Moderator at: 12/15/2021 08:46:23New subject after splitting |
|
12/15/2021 12:14 PM | |
Joined: 4/29/2021 Last visit: 12/28/2021 Posts: 50 Rating: (0) |
Hello PISCEAN, Now i can understand my PLC side . But drive side how i can find X126. Pls find here i have attached my Device configuration file. and my program backup . Pls add my profibus communication in my project backup file. [snip] Regards,
AttachmentFiles.zip (731 Downloads) |
Last edited by: Jen_Moderator at: 12/16/2021 06:29:48Removed link and added files as an attachment. |
|
12/15/2021 12:20 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Puli Kutty, My organisation IT administartion dept has locked external share/cloud links as such could not access your program. But from the attached snap, you can connect DCM drives via scalance switch port connection & assign IP address. What problem do you face doing so? |
12/15/2021 12:40 PM | |
Joined: 4/29/2021 Last visit: 12/28/2021 Posts: 50 Rating: (0) |
Hello, I want to connect Profibus communication . Scalance for only profinet . In that Profibus X126 how i can connection ? Pls how tomake a device configuration in profibus. regards,
|
12/15/2021 2:57 PM | |
Joined: 7/7/2010 Last visit: 10/7/2024 Posts: 15270 Rating: (2422) |
What have you tried in the Devices and Networks tab in the project's Devices section? Have you tried the drag and drop method of drawing connections between PB devices just like you do for PN devices? Have you reviewed the various device properties of the PB devices / modules so you could assign the PB address and communications parameters? Have you tried anything?
|
science guy |
|
This contribution was helpful to2 thankful Users |
12/16/2021 5:45 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Puli Kutty, Why you want to configure PROFIBUS when you have PROFINET available at PLC & drive side? Moreover have you read my 1st reply in this topic? In it I mentioned that to connect drive with PLC 1214 on PROFIBUS network, CM 1243-5 communication module is required. Have you noted it. Also please get this point confirmed from your local Siemens support center. Hope this helps. |
Follow us on