5/15/2014 11:01 PM | |
Posts: 5225 Rating: (1191) |
Whomever decides to weight in on this.. Messages that are open are.. V16.3 V18.4 V18.3 V18.2 Careful that V16.3 is empty, but is referenced with a ranged bit reset. The others should be fine. Muds, I would be very careful in publishing such a program in public. My suggestion is to have a password on the ZIP file and private message Marcjan the password. Please see the x2 JPGs inside the attached ZIP file. This will give you a clue to how to do it yourself. Follow the NEXT buttons until you reach the information section. Page through the pages until you reach the empty pages (52 -54). If you energise the "message enable bit" written with the message, the message will appear. In my case............... I6.5 V18.4 ---| |----------( ) Does this help you? w Attachmentvisual clues.zip (340 Downloads) |
Follow us on