8/24/2020 8:20 PM | |
Joined: 3/11/2020 Last visit: 10/27/2022 Posts: 1 Rating: (0) |
I have a DCC project built in TIA V16 that I'd like to compile. However, the DCC programming manual section 3.6.2 explains that the DCC charts can be compiled only after saving on STARTER/SCOUT. Is there a way I can migrate the Startdrive to Starter instead and compile, or should I create a whole new project on STARTER portal with reference to the STARTDRIVE DCC and then compile? Also does it still need that I go online with the hardware? Any guidance or cross reference would be much appreciated. Thank you.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/25/2020 07:51:49New subject after splitting |
|
8/27/2020 2:12 PM | |
Joined: 10/11/2006 Last visit: 5/27/2024 Posts: 5853 Rating: (793)
|
Hello,
to which manual do you refer? I think you use the old manual for Starter and not the one for Startdrive? Having Startdrive V16, you don't need Starter for DCC at all. There is also no possibility to 'downgrade' a DCC chart created with Startdrive for use with Starter. Note: with DCC V16, you don't need to manually start a compilation and there is no button to do so. |
Last edited by: Technology Team at: 08/27/2020 14:17:31With best regards, |
|
Follow us on