10/7/2018 10:49 PM | |
Posts: 2 Rating: (0) |
-Operating System: Windows 7 Professional - TIA Version : V14 - Hardware Modules numbers : S7-1214FC CPU 6ES7 278-4BD32-0XB0 IO Link Master Balluff Smartlight : IOL-802-102-Z037 - The desired application : Configure IFM IO Link master through the Siemens S7-PCT in the same way as Siemens IO Link Master is configured. Create new color+blinking preset profiles for the Smartlight and toggle the profiles based on digital inputs to the S7-1200. - The Problems (Bugs) : When right clicking on the IFM AL11100 IO Link master port, the "Start Device Tool" is greyed out which would open S7-PCT. When right clicking the Siemens brand IO link master block, "Start Device Tool" is active and it can be configure with S7-PCT. Does the IFM AL1100 IO Link Master support configuration with the STEP7-TIA portal? |
Last edited by: BMello at: 10/7/2018 10:51:18 PMLast edited by: BMello at: 10/7/2018 10:52:00 PM |
|
10/8/2018 12:39 AM | |
Joined: 9/27/2006 Last visit: 5/25/2024 Posts: 12257 Rating: (2668) |
Hello BMello; This quote from the S7-PTC v3.5 launch might interest you: https://support.industry.siemens.com/cs/us/en/view/32469496 The Port Configuration Tool ("PCT") is a PC-based software for parameterizing Siemens IO-Link master modules and third-party IO-Link devices. The IO-Link devices are integrated using the standardized device description "IODD" which can be obtained from the relevant device manufacturer. S7-PCT supports both IODD versions 1.0 and V1.1. The IFM IODD file you need can be found here: Hope this helps, |
Last edited by: dchartier at: 10/8/2018 2:21:45 AM |
|
6/5/2019 5:13 PM | |
Joined: 6/1/2010 Last visit: 1/17/2023 Posts: 36 Rating: (4) |
Hello To configure the IFM AL1100 and the IO-LINK device attached you need the paid version of Line Recorder from IFM https://www.ifm.com/us/en/category/055/055_070/055_070_010#!/S/BD/DM/1/D/0/F/0/T/24 reference IFM QA0011 et QA0012 in my country IFM propose starter kit ZZ1350 & ZZ1120 I made the configuration for the IFM AL1102 last month. Next month we try in production. PS: you can make the configuration inside TIA portal but it must be the runtime of the CPU from siemens who configure the device IO-LINK via FC FB (I did not try yet). it is looking a little difficult and complicated for the first time. |
This contribution was helpful to1 thankful Users |
Follow us on