11/2/2021 11:39 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS-Forum-Community, the SIMATIC S7-1200/ S7-1500 supports the communication with Modbus/TCP. The following application example is available for this: The application example describes the communication between a S7-1500 and a S7-1200. Both controllers are parameterized as client and as server. How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs? The Modbus/TCP server uses port 502 by default. Which ports you can use and how many clients a server can serve is described in the following article: In the manuals you will find more information about the Modbus/TCP communication: SIMATIC S7 S7-1200 Programmable controller Overview of Modbus RTU and Modbus TCP communication Hint: Modbus/TCP can be done via the local interface of the CPU or with an Ethernet CM/CP. The CM/CP must support the open communication with TCP/IP. No additional license is required for Modbus/TCP communication. This applies to the SIMATIC S7-1200, ET 200SP CPU and S7-1500. The procedure described in this article refers to the time of writing this article (status: November 2021). With kind regards SIMATIC International Technical Support Hub |
Follow us on