3/11/2014 6:02 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Wuestenraeuber We are using the FOllowing Software Versions : 1. STEP7 Professional V5.5+SP3 2. Mobus TCP/IP for PN CPU V 2.4 ( from CD Received ) 3. Modbus TCP Wizard V1.4.1 ( Downloaded from Support ) NO we didi not manually change the MODBUS_PARAM DB. If fact we create the DB using wizard and immediately restart the Wizard, it still does not detect the DB just created, although DB exists in the STEP7 program and also works normally. The only change we did was that we re-numbered the DB2 and DB3 as DB 102 and DB 103 as DB2 & DB3 were already in use in our progrem. Regards Navnag |
There is no such thing as the last bug in a program |
|
3/11/2014 8:36 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello Wuestenraeuber The Problem got solved after we executed "Check Block Consistancy" and "Compile All" No errors were noticed in Compile. Now the Wizard is detecting the DB. Thanks & Regards Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
Follow us on