3/14/2024 9:46 AM | |
Joined: 6/16/2022 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
Hello, we have a problem with the PLC/HMI connection. The PLC reacts in TIA and in the physical experimental plant but on the HMI screens the buttons don't react at all. https://support.industry.siemens.com/forum/es/en/posts/mtp-1000-connection-to-plc-issue/286461?page=1&pageSize=10 After reading this post and followed the suggestions we I haven't fixed it yet, we aren't sure why it doesn't work. I'll attach an image of the connections of the project. |
Last edited by: McFearless at: 03/14/2024 09:48:37Last edited by: McFearless at: 03/14/2024 09:53:12Last edited by: The Helping Hand at: 03/15/2024 10:01:23Link optimized |
|
3/14/2024 9:47 AM | |
Joined: 6/16/2022 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
Here is another picture of the PLC/HMI configurations. |
3/14/2024 9:51 AM | |
Joined: 6/16/2022 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
We are using the port X2 on the HMI and it is also configured in the network topology |
3/21/2024 9:16 AM | |
Joined: 6/16/2022 Last visit: 4/15/2024 Posts: 9 Rating: (0) |
Hello Stefan, The configured device version of the MTP and the image version installed on the MTP AttachmentAnswers.pdf (11 Downloads) |
3/25/2024 1:22 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651)
|
Hello McFearless yes I think this could be a matter of certificates: https://support.industry.siemens.com/cs/de/en/view/109800515 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on