10/5/2022 7:24 PM | |
Joined: 10/5/2022 Last visit: 2/17/2023 Posts: 1 Rating: (0) |
Hola a todos Soy nuevo en esta plataforma Estoy buscando la biblioteca "LOpenUseComm" para TIA Portal V13, requiero el Bloque de Función (FB) "LOpenUserComm_IsoOnTcp" para realizar una comunicación con una HMI de la marca Beijer modelo X2 pro 7, bajo el protocolo SIEMENS S7 ISO-on-TCP ¿Alguien sabe donde puedo encontrarlo? Gracias ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2022 03:46:54New subject after splitting |
|
10/6/2022 4:29 AM | |
Joined: 1/21/2013 Last visit: 4/26/2024 Posts: 2714 Rating: (440)
|
Hi elglez, you can find the required function block in the library 'LOpenUserComm'. Please note that this library is no longer updated. The same and further functionality can be found in the Libraries for Communication. Kind regards |
10/6/2022 8:12 AM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4455 Rating: (931) |
See the attached SCL file. Import this to your project. This code is modified from the Siemens' version and has been running for some years. The original Siemens version did not compile.. even the one for Step7 V16 still does not compile. You will have to ask Siemens' support team if you want the original code working with Step7 V13. You can use the "Support Request" link. Regards.
AttachmentIsoOnTcp.zip (150 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on