9/13/2018 8:30 PM | |
Joined: 1/12/2018 Last visit: 12/3/2023 Posts: 11 Rating: (0) |
I have a VMC with an 808D Advanced Milling controller. I'm trying to write a routine to clock the spindle to given degrees so I can run a broaching operation. Every time I try to issue the commands using either "M19" or "SPOS=xxx" I get an error of "025050 Axis MSP1 Contour Monitoring" The syntax I'm using is as follows: The diagnostic guide says to check two values: As part of my ATC program, I see there is an M31 command, and testing that in the MDA it is setting the spindle to a fixed orientation, and holds it (somewhat) in place. This never throws an alarm, and while the spindle holding power isn't what I would call terrific, it is orienting and holding. I CAN move it slightly by hand until the controller fights back and tries to hold it in place. I can also put a wrench on it and move it maybe 2-3x as far, and am met with a corresponding amount of force to try and keep the spindle oriented. When I let go it then overshoots and returns to position. Not far, but it IS trying to set the degree and is trying to hold it. Try as I might, exploring inside of the controllers settings and values, I can't find anywhere that the M31 command is defined, or what it's doing. Nor can I find any incantation of M19 or SPOS which doesn't alarm out. Attachmentimages.zip (212 Downloads) |
Last edited by: Jen_Moderator at: 9/14/2018 11:12:28 AMRemoved links and added files as an attachment. |
|
9/19/2018 2:54 AM | |
Joined: 7/8/2014 Last visit: 7/11/2024 Posts: 5 Rating: (0) |
Try to reduce acceleration and jerk. |
9/19/2018 8:49 AM | |
Posts: 672 Rating: (57) |
Hi, Try M3 S10 G4 F2 SPOS=90 Pee |
Follow us on