2/23/2022 8:26 AM | |
Joined: 9/16/2021 Last visit: 2/8/2024 Posts: 30 Rating: (2) |
Hello all, Currently we are forced to work with the latest COMOS licence so we can only work with PAA v3.1.1( or COMOS 10.4.0). We have a project on an old DB v10.2.2. Since we are so far ahead in the project and a bit of customizing is done, the effort to migrate the whole project is too time consuming. The thing is the database successfully opens with PAA v3.1.1 and we can do all our work except when we need to use PAA HW Configurator. Since we want to create new stations and use other PAA tools. When we open the HW configurator and go to any ET station tab and click any drop-down list, they all come empty(refer the attached screenshots). and the structure of project is also chosen based on PAA requirements(from beginning) and all the relevant base Objects are in correct hierarchy. If anybody has the similar issue or anybody knows any solution, it will be really helpful. AttachmentPAA HW Config.zip (101 Downloads) |
Follow us on