8/13/2010 3:27 AM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Nikolay, There are two serial ports on the CPU. Do you have PG interface on the second serial port so you can try to connect via that one? Regards, Behnam www.sigmaprocess.ca |
8/13/2010 6:23 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
Nikolay, 1. You should be able to use both your PC and PG to connect to CPU directly without any other interface between. 2. As you have mentioned, 6ES5734-2BD20 can only be used with PG. I have the attached the manual for CPU948. Take a look at chapter 11. Regards, Behnam www.sigmaprocess.ca/blog AttachmentS5-155U-CPU948.pdf (94 Downloads) |
9/2/2014 7:55 AM | |
Joined: 3/2/2007 Last visit: 5/27/2024 Posts: 930 Rating: (5) |
how did you solve this problem ? |
... thank you ... |
|
Follow us on