6/28/2024 6:29 PM | |
Joined: 2/1/2010 Last visit: 9/4/2024 Posts: 149 Rating:
|
I'm not able to reproduce but I only had a 9.1SP1 handy at the moment for runtime. It's working fine there, so its either hyper specific to 9.1 SP2 runtime issue which doesn't show from PDL config, or its a different issue. Are you using 9.1 SP2 APL library or an older one in the compat table? One thing I'm thinking of is the inherited permissions and data format don't match between MotL and PIDConL faceplate when derived from block icon since those are passed parameters for many APL entry boxes. Are the MotL block icon and/or PIDConL faceplate standard or customized? example, Have you changed the AnalogValueFormat1-4? 9.1SP1 & SP2 default faceplate only applies Format 1 & 3 to Deadband and Control Zone. Have you customized it to use format for also Gain? |
If my post helped you, please rate. Thanks. |
|
Follow us on