Industry Online Support
Technical Forum
12/14/2011 9:39 PM | |
Posts: 1 Rating: (0) |
Hi a customer is having serious problems configuring the G120C with the next specifications: Control via Digital inputs Setpoint via Profibus DP I suggest put the Pto 7 and the 922 to 999. Put the P840 to 722.X and send via profibus 047E and put the on/off input to control it. Other way is to put all the P848.... to1 and send nothing via Profibus in the control word. Have anyone thet it? tomorrow i will test it, i think it works. Attachmentmodif_Laborda.zip (138 Downloads) |
12/16/2011 10:57 AM | |
Posts: 739 Rating: (55)
|
Hi, there is a hard ware and a software change between V3.xx and 4.4. This versions are not comparable. For information see FAQ: What do I have to observe, if I want to replace a CU240E of the SINAMICS G120 with a CU240E-2 (firmware V4.4)? http://support.automation.siemens.com/WW/view/en/54997738 What do I have to observe if I wish to replace a member of the CU240S family (CU240S, CU240S DP, CU240S DP F, CU240S PN or CU240S PN F) of SINAMICS G120 by a CU240E 2 (Firmware V4.4)?http://support.automation.siemens.com/WW/view/en/55644272 |
Follow us on