Industry Online Support
Technical Forum
11/6/2013 9:04 PM | |
Posts: 7 Rating:
|
Hello, I want to use any OPC server and make vizualization of the sw control on the PC screen. |
11/7/2013 2:23 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating:
|
yes this is possible. you just have to setup the pc station with the opc server and then add in netpro a connection between the et 200s cpu and the opc server (e.g. s7-connection). the following manuals are useful for opc: 1. and 2. |
Best Regards, |
|
Follow us on