12/15/2022 9:22 AM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2879 Rating: (460) |
Hi Wayse2, since in WinCC Unified all positions and sizes are specified in pixels, I would also use pixels for SVG. Your description makes me think of the 'viewBox' attribute. Please check, if there values are matching the width and size parameters. You can post your SVG file here and I - or someone else - can take a look on it. Kind regards |
12/15/2022 10:30 AM | |
Joined: 11/24/2022 Last visit: 3/13/2024 Posts: 19 Rating: (0) |
Thank you for the information . viewbox might be an issue , but only one of the object is out of the view box. i have attached the file with this message .
Attachmenttest.zip (232 Downloads) |
12/16/2022 10:35 AM | |
Joined: 1/21/2013 Last visit: 6/12/2024 Posts: 2879 Rating: (460) |
Hi Wayse2, I have tested your SVG file with WinCC Unified V17, Update 5. I could not find any problems, neither in the engineering, nor in the browser (Google Chrome) or on a MTP700. I have seen, that the SVG file comes without hight and width parameters. Maybe it will improve the behaviour when adding those parameters. For a more detailed understanding of your issues, please post some screenshots. Kind regards |
Last edited by: Stefan Arcularius at: 12/16/2022 10:36:16Typo corrected |
|
This contribution was helpful to1 thankful Users |
Follow us on