3/14/2019 8:26 AM | |
Posts: 19 Rating: (0) |
Good day, experts. I've tried doing the suggestion above, I don't understand why the simple program doesn't work. Basically, I have two identical antennas, (RF620A) connected to a reader (RF680R). My test program works with when only one antenna (or technology) is in the program, but not two. Makes sense? I made sure I assigned two different channels on each HW_CONNECT (Ident_1 and Ident_2). whenever I have both FC (each FC containing the READ and WRITE blocks for RFID with two unique channels and technology each) in the program, the reader always output an error. Does anybody know the solution to this? Help Kervs ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/14/2019 9:03:53 AMNew subject after splitting |
|
3/14/2019 9:49 AM | |
Posts: 19 Rating: (0) |
<solved> realized I have just copied the block and didn't configure the READ/RESET/WRITE DB's. |
This contribution was helpful to1 thankful Users |
Follow us on