3/28/2007 2:12 PM | |
Posts: 39 Rating:
|
Hi Can i use more than 7 RTM (SFC2,SFC3,SFC4) in a CPU? why i can not use SFC101 in some CPU's? How can i read CP fault and send it to HMI ? thanks |
4/4/2007 7:09 AM | |
Posts: 39 Rating:
|
HI |
4/11/2007 9:46 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating:
|
Hi, SFCs and SFBs are typical for a CPU. If you want to know wich SFCs and SFBs you can use inthe CPU you're using you should do an upload of these blocks. A 'nice' example is when replacing a CPU314IFM by a CPU314C-2DP where internal functions are used. If you want to dislpay errors on Siemens HMI, you can use Report System Error (RSE). In ProTool and WinCC flexible you have to enable some options and I believe in WinCC also. For the CPU it is also quiet simple:
For more information you can see your programming manual or have a look at the support siteand the words'report system error'. |
Smurf |
|
8/22/2013 12:17 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to How can i know if the cpu has 32 or 16 bit runtime clock? Best regards O_Moderator |
Follow us on