4/16/2015 12:20 PM | |
Posts: 17 Rating: (0) |
i want to convert this fonction from s5 cpu 135u to s7 400, it's a save data fonction, after the conversion I have the following from errors: FUNCTION FC 20 : VOID NAME: SAVE BEGIN NETWORK AUF DB 118; // LRD 0; T DBD 0; // LRD 2; T DBD 4; // LRW 6; T DBW 12; // LRW 8; T DBW 16; // LRD 9; T DBD 18; // LRD 11; T DBD 22; L MD 238; T DBD 26; L MD 242; T DBD 30; L MD 246; T DBD 34; L MD 250; T DBD 38; L MW 254; T DBW 42; END_FUNCTION How i can replace "LRD0, LRD 2, LRW6, LRDW 8, LRD 9, LRD 11" in the S7 code Best regards ------------------ |
Last edited by: CS Moderator at: 4/18/2015 5:06:47 PMnew subject after splitting |
|
4/18/2015 5:10 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
closed cause question published twice.
The second thread with the subject S5 135U s5 to s7 conversion Errors is published within the same conference.
Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on