10/5/2017 11:44 AM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
Hi All, Waiting for feedback. AttachmentFault_400Cpu.zip (211 Downloads) |
Last edited by: RAKIB at: 10/5/2017 12:20:35 PMLast edited by: RAKIB at: 10/5/2017 1:38:16 PMLast edited by: RAKIB at: 10/5/2017 1:48:26 PM |
|
10/5/2017 3:21 PM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating:
|
For newer CPUs , it is possible to update both via flash memory and the Hw.Config.You will find more in the following link: Operating system updates V6 CPU412-5H PN/DP, CPU414-5H PN/DP, CPU416-5H PN/DP, CPU417-5H PN/DPPlease,
I hope it helps, hdhosseini |
This contribution was helpful to
1 thankful Users |
12/14/2017 7:08 AM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
Dear hdhosseini, Hi. I have updated the Firmware Version of the Cpu 6.0.4 ti 6.0.6. now the two cpu has same firmware version 6.0.6. But the problem is still there. i have attached the present module information and hardware configuration of the project. Please have a look on them and suggest me what should i try to solve the problem? Thanks Rakib AttachmentHARDWARE_CONFIG_NEW.zip (178 Downloads) |
12/14/2017 7:09 AM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
Here is the module information.
AttachmentModule_information.zip (181 Downloads) |
12/14/2017 11:18 AM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating:
|
Hello again, Thanks for your feedback. For an H-CPU there are certain OBs that should exist to avoid CPU entering the STOP mode.Please,include all in your program.You can search THIS manual for more information. There is a simple instruction to set up the entire H-system in page #40 of THIS manual.For your test, include an OB1, error OBs , delete all external I/Os and set correct rack number.In the first step you can remove Flash cards on the CPU for simplicity (when each CPU is in STOP or off). If any problem exists , please share the diag buffer of each CPU in text format. I hope it helps, hdhosseini |
Follow us on