5/31/2015 11:37 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308) |
Hello ubv29, 1- As far as I know the memory compression should not change the CPU to stop. 2- It differs from one to another but I would recommend at least 40% memory space in work memory. 3- First, what is the part number of your CPU and what is the type and size of your memory card? Maybe, you can solve your problem with larger memory card and maybe you need to change your H-Station to the latest V6 S7-400H. Best regards, H-H |
6/1/2015 6:47 PM | |
Joined: 5/20/2015 Last visit: 10/8/2024 Posts: 34 Rating: (15) |
CPU Part is 6ES7 417-4HL04-0AB0 |
Follow us on