8/12/2008 10:22 AM | |
Posts: 37 Rating: (0) |
...more clear and shorter - where in S5 can I set the SAP numbers? |
Last edited by: plenc at: 8/12/2008 10:23 AM |
|
8/12/2008 12:18 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, What S5 system do you use? For a CP5430/31 the connections and SAPs are setin the CP with COM5430 or COM5431 when you use a CP5430 or CP5431 If you useopen FDL services, you the destination SAP and destination address is set in DBs. The useful data is preceded by a request header in the DBof the PLC, and you must fill the header with SAP and destination address for instance. Have a look to thesemanuals: CP5430-31: http://support.automation.siemens.com/WW/view/en/1804226 95U-FDL: http://support.automation.siemens.com/WW/view/en/1091429 Old manual WinCC V5: http://support.automation.siemens.com/WW/view/en/1405762 In chapter 9, there is an explanation of an FDL connection with S5-115U , with an older CP5412, but the PLC part could be usefull. From chapter 9.2: "These are the standard function blocks FB9 L2STARTUP and FB10 L2SNDRCV. They must be transferred into the STEP5 program. The blocks support 5 different FDL connection instruction types. For each of these instruction types, a predefined work-DB is available, which contains various message data." I hope this help. |
Best regards |
|
8/12/2008 5:34 PM | |
Joined: 10/12/2006 Last visit: 5/7/2024 Posts: 206 Rating: (25) |
hi plenc, sorry that was my mistake it isn't H1. Best regards Zenta |
Last edited by: Zenta at: 8/13/2008 9:16 AM |
|
8/13/2008 8:52 AM | |
Posts: 37 Rating: (0) |
Hi, Pleasecheck attached document. In dok1.doc there are screens from my NCM configuration but i still don't know which SAP number should be set in which gap in WinCC connection paremeters window (wincc_parametrization file from attachment). Please show me how to fill it. Best Regards, P. AttachmentSAP_number.zip (103 Downloads) |
8/13/2008 10:20 AM | |
Joined: 10/12/2006 Last visit: 5/7/2024 Posts: 206 Rating: (25) |
|
Last edited by: Zenta at: 11/18/2008 1:06 PM |
|
Follow us on