8/26/2018 12:54 AM | |
Joined: 9/27/2006 Last visit: 5/23/2024 Posts: 12257 Rating: (2668)
|
Hello hamad; What kind of memory card are you using in the CPU? RAM or Flash EPROM? If using a RAM card you need battery support to maintain the program in memory. Simply downloading the program to the CPU will place it in the RAM card. If using a Flash EPROM card, your program will be maintained without battery support, but to download you need to place the CPU in Stop mode and use the Step 7 function "Load program to memory card". You will have more complete information in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/7302549 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/26/2018 12:55:23 AMLast edited by: dchartier at: 8/26/2018 12:57:37 AM |
|
This contribution was helpful to1 thankful Users |
8/29/2018 12:52 PM | |
Joined: 5/8/2016 Last visit: 2/15/2024 Posts: 167 Rating: (13) |
hello its done by doing as explained in the image attached |
A lot of potential remains |
|
Follow us on