Industry Online Support
Technical Forum
6/24/2013 12:39 PM | |
Posts: 12 Rating: (1) |
Hi, Im a new user of s7 1200 and seeking for support in hosting. First, some users/advicers recommanded using port forwarding with port 80 and port 443. Well, I tried but not working at all so I decided to open a new post and request for more details. here is my IPs setting. PLC IP: 192.168.0.10 Dlink IP: 192.168.0.1 Subnet: 255.255.255.0 1) While I configure my dlink router (dir615), it says both ports are used and does not allow me to save the setting of my router. So I tried port 85 and 444, just a random pick number, and other ports such as 48111, 3287.....etc, well, the router allow me to save the setting, but of course, it is not working. 2) I doubt, the problem might not from the port, so I tried on the DMZ, disable all the dos attack and scan attack protection. Guess what, it is not working as well. Since DMZ is a place that allow all ports to enter, I guess this prove the problem is not from the "port" thing. :P 3) Im currently using the dlinkddns.com because it provided 1 free account for dynamic IP server, please refer to the "ddns setting.jpg" . I guess the ddns account is activated and the service is running since I got a "successfully updated" while I click on the "ddns account testing". Of course, I also tried to insert a wrong password and I got a "failed to update", this prove the system is really running, refer to "ddns setting failed.jpg" Regards Lian
Attachment240613.zip (23 Downloads) |
Follow us on