10/1/2019 7:04 AM | |
Joined: 1/25/2010 Last visit: 3/15/2024 Posts: 10 Rating: (1) |
Recently I am facing an error indicate that the Data Block generated by SFC Function Block is outside of user range whenever I modify any SFC and perform Program Changes download. The Data Block generated by SFC suppose to be system data block instead of user data block. However, I managed to overcome this error by performing full compilation and program changes download. But this is very troublesome. Wondering if any of you facing similar issue before? Note: I am using PCS 7 V9.0 SP1. AttachmentSFC Error.pdf (79 Downloads) |
This contribution was helpful to2 thankful Users |
10/1/2019 7:27 AM | |
Joined: 3/14/2008 Last visit: 6/4/2024 Posts: 2070 Rating: (928)
|
Hi chiawc, Yes, I've had that problem once and several forum members as well. You got off the hook easily, I had to do a whole update of CFC and afterwards full compile+download. This problem exists in V8.1 as well. But thanks for providing your solution! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on