9/7/2022 9:24 AM | |
Joined: 4/22/2020 Last visit: 10/11/2024 Posts: 4 Rating: (1) |
Hello everyone I am setting up a Fritz Werner TC630 With Sinumerik 850m, Machine Number 816480, but I don't have the basic parameters. After loading the parameters of NC MD, PLC MD, one of the machines that is similar to this machine and is in the attached file, all the axes go to reference except Magazine and the spindle does not rotate with the handwheel. It is necessary to explain that there are 6 similar devices with Sinumerik 850&880 controls and they are working. Help me please. AttachmentTc630-02.zip (337 Downloads) |
Last edited by: The Helping Hand at: 09/08/2022 07:51:25Changed thread title for more clarity |
|
9/9/2022 1:17 PM | |
Joined: 4/22/2020 Last visit: 10/11/2024 Posts: 4 Rating: (1) |
Hi I am in the process of setting up a FRITZ WERNER TC630 Sinumerik 850 machine with machine serial number 816480 and there are 6 similar machines available. I have attached all the information and plc programs of the similar devices in operation and the device that is being started in my message in the thread. The plc of these devices is of the simatic s5 150u type and its programs are on EEprom, because the overall structure of the devices is similar It is the same and the only difference is in the serial number and an additional input rack, and we don't have a backup of the nc and plc data of the device while it is being set up. The electrical map is not available for this machine and we used the electrical map of devices similar to this machine and their parameters to set up, and we were able to reference all axes except the magazine, if you have the nc md and plc md parameters of this machine model available or Can you help in analyzing and launching the magazine? Please let me know. Thanks
AttachmentTc630-02.zip (320 Downloads) |
Last edited by: Hadi0291 at: 09/09/2022 13:19:18 |
|
Follow us on