Industry Online Support
Technical Forum
10/26/2009 12:45 PM | |
Joined: 7/8/2009 Last visit: 9/20/2022 Posts: 56 Rating: (0) |
Hello Guys i have a question i have 2 PC Stations The First one has WINCC Installed to it the Second one has Simatic MangerWith Simulator i have to Connect the WinCC Station to the PLC "simulation" i have done the NetWork Configuration But i i can't establish the Connection May be it is not Possible to do this Connection Please guys help me with this Situation to make it easy to understand me i attached snap shots of all the Configuration i made Thanks AttachmentWINCC , PLC SIM.pdf (39 Downloads) |
10/27/2009 9:24 AM | ||||||
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Cheetos , here link for previuos tread:
Hope can be useful Regards |
|||||
Follow us on