5/13/2016 7:11 AM | |
Joined: 6/11/2007 Last visit: 5/31/2024 Posts: 61 Rating: (7) |
Hello GREY you should visit following link where you can find lot of application desciption for controlling of sinamics from S7-300/400 PLC Following link will make you clear how control and monitoring of drive takes place with control and status word resp. Application examples for Sinamics over Profibus Don,t know how integration of Sinamics VFD with PCS7 V6 takes place but it should be possible. Once you know how the actual mechanism works then you should be able to control the VFD with PCS7 also. In PCS7 V8.0/V8.1 the actual block we use to control the motor is MotSpdCL. PCS7 V6 should have some motor block to control the speed controlled motors and if you know the mechanism you can implement further logic. |
Thanks |
|
Follow us on