2/19/2021 3:36 AM | |
Joined: 7/1/2013 Last visit: 8/14/2022 Posts: 9 Rating: (0) |
Hi, we have a Knuth CNC machine using the Sinumerik system but at this moment it is in defect mode showing alarms 'PROFINET - I/O ramp-up fault type: 1', 'PLC STOP 3', 'Emergency stop', 'PLC sign-of-life monitoring ' I believe it's related to software problem. The problem came after 2 weeks of quarantine, then when the operator came back to work and switched on the machine, these alarms came out. Thank you in advance for your assistance. AttachmentXmill1100_alarm.mov (103 Downloads) |
Last edited by: alfred751112 at: 02/19/2021 05:04:36 |
|
2/19/2021 5:06 AM | |
Joined: 7/1/2013 Last visit: 8/14/2022 Posts: 9 Rating: (0) |
Rear panel LED's. |
2/19/2021 8:12 AM | |
Joined: 7/1/2013 Last visit: 8/14/2022 Posts: 9 Rating: (0) |
Hi PISCEAN 2010, it's in the first message in this topic. I edited and put the video in there. |
2/19/2021 10:26 AM | |
Joined: 7/1/2013 Last visit: 8/14/2022 Posts: 9 Rating: (0) |
Rear panel LED's (video)
Attachment20210217_110244.mov (107 Downloads) |
2/20/2021 4:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, Do you have set up archieve data back up on external device of on CF card? If yes you need to restore it. |
Follow us on