Industry Online Support
Technical Forum
9/29/2011 11:34 PM | |
Posts: 24 Rating: (0) |
Maybe you can help me with another timer. It's a T!-!0 timer ( TON ) But it is activated by de Not M10.0 value. The Q value of the timer set M10.0 value. I think it is wrong , the timer never can count to the TW value. It is active one cicle and off the next. Is this correct ? This is the code of the segment :UN M 10.0 :U( :UN M 10.2 01 :U( 01 :U( 02 :UN M 10.0 03 :L KT 035.0 03 :SE T 1 03 :NOP 0 03 :NOP 0 03 :NOP 0 03 :U T 1 03 :) 03 := M 10.0 02 :U M 10.0 02 :) 02 :S M 10.1 01 :U M 10.0 01 :U M 10.2 01 :R M 10.1 01 :U M 10.1 01 :) 01 :S M 10.2 :UN M 10.1 :UN M 10.0 :R M 10.2 :NOP 0 :*** Regards Fernando Splitted from Migrate S5 101U to S7-200. |
Last edited by: O_Moderator at: 9/30/2011 8:23 AMnew subject after splitting |
|
Follow us on