Industry Online Support
Technical Forum
10/21/2014 11:21 AM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
Do you have a connection between the negative terminal of the battery and the M terminal of the LOGO !? According to the data sheet of MCP9700A are between a temperature of -40 ° C and +125 ° C from a voltage of 2.3 V to 3.95 V. Example, see attached file. AttachmentExample TS01.zip (152 Downloads) |
10/22/2014 4:11 PM | |
Posts: 2 Rating: (0) |
Thanks!It´s working now!. |
This contribution was helpful to1 thankful Users |
Follow us on