9/22/2022 10:49 AM | |
Joined: 2/17/2020 Last visit: 10/31/2024 Posts: 1105 Rating: (200) |
Hi ro14, Please try to delete the IM folder, recompile the HMI in the project and download the project to the UCPs again. Note: it is important to also have the latest TIA V17 Update installed and configure the maximum configurable image version for the UCPs. If this doesn't work... do you use any script to show the time in the IO Field? Could you attach it? |
A rating will be well appreciated. |
|
Follow us on