3/6/2012 7:24 AM | |
Posts: 33 Rating: (0) |
Dear Darious That is the problem we dont have the original project and there is no other option to upload it from the panel |
3/6/2012 7:32 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Well, you can do an upload using Prosave, but in that case you can only restore it into the same type of the panel. I think you can still order that type of the panel from Siemens as a spare part. So I think it's very good idea to make backup of the panel just in case. How do you backup/restore with a Windows-based panel? |
Best regards, |
|
Follow us on