4/3/2024 6:52 AM | |
Joined: 1/19/2017 Last visit: 4/23/2024 Posts: 9 Rating: (0) |
I'm running into the same issue, no solution is given in the posts pointed to. I've got 30 SIWAREX modules in my current project and just figured out that the Siemens provided FB (WP321DR) is optimized now thus multiplexing from my MTP2200 Unified panel isn't an option anymore. I've found different ways of going about this but none of them talk about Unified and multiple SIWAREX modules. I'm not real eager to create all the tags needed for SIWAREX times 30 and link them all individually, there must be a better solution right? Anyone have any ideas? Kind regards, Daniël ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/04/2024 11:34:24New subject after splitting |
|
4/11/2024 6:59 AM | |
Joined: 8/3/2009 Last visit: 5/15/2024 Posts: 12951 Rating: (1649)
|
Hello Echo[NL] I´m not sure if you can use this for the SIWAREX but since TIA V19 you can use Dynamic Tag Names in Interface of Faceplates (you would have to create all Tags but you will be able to use also PLC UDTs): (Here is an general Example for SIWAREX, don´t know if you already know: https://support.industry.siemens.com/cs/de/en/view/94109373 ) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on