12/9/2022 8:06 PM | |
Joined: 5/21/2017 Last visit: 4/20/2024 Posts: 15 Rating: (2) |
Hi In V18 i can see Pro versions of unified comfort panels But i couldn't find any info what are those, anyone? |
12/9/2022 8:42 PM | |
Joined: 9/27/2006 Last visit: 6/11/2024 Posts: 12260 Rating: (2670) |
Hello Kamil; Look at this information from the Siemens Industry Mall: https://mall.industry.siemens.com/mall/en/ww/catalog/products/10087316 Hope this helps, Daniel Chartier |
12/10/2022 4:02 PM | |
Joined: 9/27/2006 Last visit: 6/11/2024 Posts: 12260 Rating: (2670) |
Hell Kamil; The screenshot in my last post icluded a presentation link that shows the Unified Pro panels with more details: The document states that besides the IP 65 ingress protection lebvel, the panels are designed for installation on a mounting rm or a support foot, so they can be installed directly on a machine environment, without cabinet. Also, the Unified comfort PRO panels description accessed from the same document shows that they are programmable from WinCC v14 SP1 (with HSP) and higher, so WinCC v18 should refer to exactly the same panels... Hope this helps, Daniel Chartier |
Follow us on