12/29/2014 8:47 AM | |
Posts: 567 Rating: (106) |
Hi, the following information you can find in the siemens industry mall: " Note on the upgradeExisting installations from CEMAT V6.1 upwards can be upgraded by means of the CEMAT software upgrade V8.0 (SP1 incl.). The upgrade from CEMAT V6.1, V7.0 or V7.1 also incorporates a WinCC user archive upgrade, so one CEMAT software upgrade is required for each engineering station, OSserver and OSsingle station. To upgrade CEMAT V8.0 to V8.0+SP1, however, only one CEMAT software upgrade per plant is required." |
Follow us on