8/31/2011 8:55 AM | |
Posts: 2964 Rating: (484)
|
Hello.... You can use.......does your 840D is equipped with PCU50 / PCU20? If it is PCU50 you can configure this information on screen itself....if it is PCU20 you need to have Laptop in that you should have HMI advanced PC/PG from there you can configure it... check this link regarding configuring the power module...hope this may find it useful /tf/WW/en/Posts/56743#top Regards, Prakash |
9/1/2011 6:21 AM | |
Joined: 6/18/2008 Last visit: 3/3/2024 Posts: 108 Rating: (0) |
Hi. Thanks for reply I know procedure drive configuration but i want to know installation : *** 3 **** power module with *** 2 **** control unit(control unit1 ->1axis , control unit2 ->2axes) You suppose i install 3 power module in mountig surface first. Now i have fowllowing questions 1- where do position of power modules , Control unit 1 and 2 have to install? (I emphasize, i have 3 power moude with 2 control unit) 2- How do i configure power module and control unit in drive config screen? 3-which does power module each power cable of motor have to connect? Thanks. |
9/1/2011 8:48 PM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
This configuration is exactly as the example in the doc on cd AttachmentStart-Up Guide 840D_810D_611D.pdf (83 Downloads) |
Follow us on