6/30/2021 5:51 PM | |
Posts: 4 Rating: (0) |
I have a CNC spindle motor from the store and i found it is a better one, high quality. Two weeks ago, I bought a CNC spindle motor in another place, I equipped with it on machine and I found it had much overheating, I checked the load, the motor cooling system, the motor cooling fan, and the connection between the motor and the control unit. However, I still failed to find out the real reason of its overheating. I want to know what else will lead spindle motor overheating so that I would take some actions to extend its service life.
|
7/8/2021 3:52 AM | |
Posts: 4 Rating: (0) |
thank you very much, I will check one by one. |
This contribution was helpful to1 thankful Users |
Follow us on