3/15/2022 2:55 PM | |
Joined: 4/14/2021 Last visit: 4/29/2024 Posts: 2 Rating:
|
Hello, at Options>>SU administration, I am able to see my SIMIT devices. I unchecked the DHCP, this allows me to enter the IP address (192.169.0.10) and subnet (255.255.0.0). P.S: I am skeptical about why I have the value "-(Wrong subnet?)" in the firmware column. There is no button to trigger the save command so I guess it is done automatically after I press OK button in the lower right corner of the SU administration window. (Attached Image 1 after performing above steps) But when I open SU administration window again, I see no change and my parameters are not saved. (Attached Image 2) Any advice for me? Regards ------------------------------------------------------------------------------------------ AttachmentImages.pdf (131 Downloads) |
Last edited by: Jen_Moderator at: 03/16/2022 09:43:58New subject after splitting |
|
3/15/2022 4:02 PM | |
Joined: 4/14/2021 Last visit: 4/29/2024 Posts: 2 Rating:
|
Solved!!! I used accessible nodes function of TIA Portal to search for the device and assign IP address. After IP address assignment the -(Wrong subnet?)" in the firmware column also replaced by an actual firmware value. |
This contribution was helpful to
2 thankful Users |
Follow us on