1/28/2017 5:37 PM | |
Posts: 3 Rating: (0) |
Hi, I have the same problem, I do not know whether to install a scada system or pcs7. I work for pharma industry (biologics). The most important point is the high reliability necessity. The production bathes are high value. I have purchased a redundant cpu, 414-5h, and I want to install a redundant pc too for the scada system o pcs7 runtime application. The systems to be controlled are: hvac system, pharma water loops, electric distribution system, chilled water loop (and chiller management), boiler and hot water loop, compressed air…all of them are critical for the production. Concerning communications, I want to install a profinet ring for machines and 414-5h, but I do not know whether to communicate the et-s of the 414-5h in double profibus or profinet ring. Thank you very much for your support. Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/30/2017 4:19:59 PMNew subject after splitting |
|
1/31/2017 10:16 AM | |
Posts: 43 Rating: (7) |
If you want store huge number of data for n number of years, SIEMENS has solution to use PCS7 system with Process Historian Application |
Follow us on