12/16/2020 10:44 AM | |
Joined: 4/28/2015 Last visit: 8/20/2024 Posts: 36 Rating:
|
Ok, the last unresolved question is why OS Compile Wizard always tries to create ISO connection with MAC address even I have configured a usual AS-OS "TCP connection" in NetPro? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2020 07:52:04New subject after splitting |
|
12/21/2020 11:46 AM | |
Posts: 198 Rating:
|
Hello RovRy, Before I can give you a conclusive answer on this, can you please provide the below details? 1. Can you please share the screenshot of the connections listed in the OS Compile wizard window? (Reference screenshot attached) 2.In your configuration for AS410, I see that the PN-IO for CP443-1 is connected to the PLC_Span_Net IE connection. Can you please share a screenshot of the properties -> Parameters tab of the PN-IO in CP443-1?(Reference screenshot attached) Usually, if 'IP Protocol is being used' is ticked and the relevant IP address is mentioned here, the same TCP connection will be visible in the OS Compilation wizard. However, with the screenshots I will have some more information to conclude. Cheers! AttachmentOS_Compile-Connections-list.zip (93 Downloads) |
Follow us on